The power density of AC/DC converter modules is increasing, but often requires high airflow rates to achieve their stated performance. However, forced cooling using mechanical fans brings reliability, noise and dust pollution issues. Baseplate cooling solves all of these problems, but only if the converter is specially designed from the outset to utilize conducted cooling measures, such as the new RACM230-G and RACM550-G series from RECOM, which delivers high power in a small form-factor along with a long list of other useful features.